How can we help you today?

SBSAD800R Seismic Information and instructions

Issue:

Needs seismic information and instructions for a SBSAD800R

Product Line:

Sped-D boards

Environment:

SBSAD800R

Cause:

Seismic information

Resolution:

The published information on seismic certification can be found under the attached SPEED-D14 & D15 drawings and its instruction bulletin (80244-812-08 page 13).

Schneider Electric Nigeria

Attachment(s)
SPEED-D15 (1).zip [2.88 MB]
80244-812-08 (8).pdf [3.29 MB]
SPEED-D14.zip [1.96 MB]