Issue:
Is it possible to display the revision number of the project in the runtime of Vijeo Designer?
Product Line:
Vijeo Designer (all versions)
Resolution:
In Vijeo Designer there is no internal variable that would give access to and allow to display the project revision number or the Buildtime and Runtime version of Vijeo Designer.
At the HMI startup, it is possible to view the project revision number as it gets displayed during the startup sequence.
On the HMI, it is possible to see the version of the Buildtime used to compile the project and the installed Runtime version by accessing the System Menu of the HMI.
To display this information on a graphic panel of the project, the workaround is to use static texts that will need to be updated by the programmer to show the correct information.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Nigeria