How can we help you today?

Control Expert returns error 'Impossible to save DTM Catalog file'.

This can occur if there are a large number of third party DTM's installed on the PC.

To resolve the issue,
  • Uninstall the third party DTM's.
  • Start Control Expert.
  • Update the DTM catalog.
  • Open or create an application.
  • Close Control Expert.
If you need the third party DTM's for Control Expert:
  • Install only the third party DTM's that are needed for Control Expert.
  • Start Control Expert
  • Update the DTM Catalog.
If you install any third party DTM's that are not needed for Control Expert, do not update the DTM catalog when
starting Control Expert.

Schneider Electric Nigeria