Issue:
How can the ATS480 soft starter run a small motor without tripping?
Product Line:
ATS480
Environment:
All
Cause:
NA
Resolution:
Small motor test setting [SST] is a parameter found under Menu 3 [Complete settings] CST then in Menu 3.3 [Motor wiring] MWMT.
This parameter can be used to perform a test using a small motor.
When set to YES the Phase loss monitoring (PHP) is disabled and the Control Mode (CLP) is forced to Voltage Control.
This will allow the unit to normally start when a run command is applied During the test, the display terminal displays the state [Small Motor Test] SST.
This parameter automatically resets to NO following a power cycle.
Released for: Schneider Electric Nigeria