How can we help you today?

P2P Communication Between Simulators in EcoStruxure Process Expert

This Knowledge base article explains the steps on how users can exchange data between the two Simulators with the help of the new implementation of Peer to Peer feature in EcoStruxure Process Expert.
The users should be able to configure the P2P to read variable values from a remote controller or write variable values to a remote controller using the specialized functions of the control participant. EcoStruxure Process Expert’s control participant provides two function blocks ‘READ_REMOTE’ and ‘WRITE_REMOTE’ which can be used to exchange the data between controllers/simulators to read and write information to the remote variables
Note: This feature is available only for the EcoStruxure Process Expert 2021 and above versions
This is applicable for EcoStruxure Process Expert 2021 and above version

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings