Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Accessories are included inside the box/packaging of Smart-UPS Ultra 8kW and 10kW 230V models (SRTL8KRM4UI and SRTL10KRM4UI)?
Issue:

There are questions regarding the accessories that are included in the packaging



Answer:

SRTL8KRM4UI / SRTL10KRM4UI-APC Smart-UPS Ultra Online Li-ion 10kVA 230V expected accessories:

Part NameManufacturing Part NumberDescriptionQty
1.BatterySRYLBMInternal battery2
2.Bezel0M-102830AFront Bezel1
3.Railing kit0M-756HRack mounting kit1
4.Litkit assy.0L9787Bmounting accessories1
5.SensorAP9335TTemperature sensor 1

See actual images

1. 2pcs of Battery Modules ( SRYLBM)- can be found at the top upon opening of the box/packaging. (see image below "Figure  A")

FIGURE  A:
Top level.JPG

2. Bezel - can be found underneath the battery packaging (see image below at "Figure B")
3.  Railing kit - can be found underneath the battery packaging (see image below at "Figure B")

IMAGE B:
bezel and railing kit.JPG

4 Lit-kit assembly - can be found at the side of the box (near the UPS)
see content below at "Figure C":

FIGURE C:
litkit assembly 1.JPG




5. Temperature Sensor (AP9335T)  - can be found near the lit-kit assembly (see "Figure D")

FIGURE D:
sensor.JPG

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: