Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the SCADAPack x70 devices' power requirements?
The SCADAPack 470 will work from 11 to 30Vdc and it is validated by Schneider Electric.

14 - 29Vdc (class 2 power supply) is the specifications that UL certified for SP470.

Power Datasheet

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: