Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a "T" fitting for the Power busbar PBCE5A225ST120B?

Issue:

Needs a "T" fitting for Powerbus busway

Product Line:

Busway

Environment:

PBCE5A225

Cause:

N/A

Resolution:

For Powerbus applications that require a tee, a cross should be used and the unused end should be

capped off

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: