How can we help you today?

Magelis HMI - Looking for a way to automatically synchronize the recipes from multiple HMI's

Issue:
Is there a way to automatically synchronize the recipes between multiple HMIs?

Product Line:
Vijeo Designer software, Magelis HMI.

Resolution:
There is no such feature already implemented in Vijeo Designer that would permit to automatic synchronization of the recipes between the HMIs,

But there are two "manual" ways to synchronize recipes between all HMIs:

1- Use a USB stick to save the desired recipe(s) from an HMI. Go over to the other HMIs with the USB key and import the recipe(s) from the USB stick.

2- Use the Vijeo Designer Data Manager application to connect to the HMIs, one after the other, and upload the recipes to the computer. Do a selection of the desired recipes to keep. Then, reconnect to the HMIs and download the selected recipes to them.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria