Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unable to change brA to Yes in ATV320.
Issue:
Why am I unable to change brA to Yes in ATV320 drive?

Product Line:
ATV320

Environment:
All

Cause:
NA

Resolution:
[Dec ramp adapt.] or (brA) is forced to [No], if the brake logic control [Brake assignment] (bLC) is assigned to a Relay or Digital Output.
The function is incompatible with applications requiring:
- Positioning on a ramp.
- The use of a braking resistor (the resistor would not operate correctly).