Why do I get the error message "Vijeo-Designer Lite version 1.3 must be installed" when installing SP1 and I already have Vijeo Designer Lite V1.3 installed?
Issue:
Error message during the installation of SP1 for Vijeo Designer Lite V1.3
Product Line:
Vijeo Designer Lite
Resolution:
The error message below is generated when Vijeo Designer Lite is installed on a non-supported operating system such as windows 7/10/11 64 bit. Vijeo Designer Lite is supported on Windows XP/ Windows 7 32 bit only.
Released for: Schneider Electric Nigeria