Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the handle force required to operate the handle of a PowerPacT H Frame circuit breaker?

Product Line: Molded Case Circuit Breaker

Resolution:
The following forces are required to operate the handle of PowerPacT H Frame circuit breaker:

ON - 14.8 lbs  (force required to close the breaker by pushing the handle from OFF to ON)
OFF - 16 lbs (force required to open the breaker by pushing the handle from ON to OFF)
RESET - 20.7 lbs (force required to reset the breaker after a trip by pushing the handle from TRIPPED to OFF)

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings