Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the altitude derating of standard TM5 IO modules?
The altitude derating of standard TM5 IO modules is the same for all TM5 modules but it doesn't mentionned on the documentation.

TM5 environmental condutions:

temperature TM5 IO modules

The TM5 altitude derating is a reduction of ambient temperature by 0.5°C per 100m:

0 to 2000m => No limitations
>2000m => -0.5°C / +100m

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings