Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I configure a Harmony HMI to communicate to a Koyo PLC?
Issue
EcoStruxure Operator Terminal Expert or Vijeo Designer HMIs do not support Koyo PLC protocol.
So, how would one go about configure a Harmony HMI to communicate to a Koyo PLC?

Product Line
Vijeo Designer
EcoStruxure Operator Terminal Expert

Resolution
Koyo PLC comm ports can be configured as a Modbus port. This would allow a Koyo PLC to be included on a Modbus network.

Koyo uses octal addressing. Attached is an Excel converter tool that converts the Koyo address to a corresponding Modbus address based on the Koyo Modbus port configuration.
Filename: "modbus_conversion.xls"

Schneider Electric Nigeria

Attachment(s)
modbus_conversion.xls [72 KB]