How can we help you today?

What are the remote/door mounting keypad and cable part numbers for ATS480?

The ATS480 is delivered with the VW3A1113 Plain Text Display Terminal (built-in).

The remote keypad, model VW3A1111 Graphic Display Terminal, is available as an optional upgrade to replace the standard Plain Text Display Terminal. Additionally, door mounting kits are offered as accessories, allowing the display terminal to be conveniently installed on the enclosure door.

The cable options are:
• 1 meter: VW3A1104R10
• 3 meters: VW3A1104R30
• 5 meters: VW3A1104R50
• 10 meters: VW3A1104R10

NOTE: The cables are not included with the remote kit.

Adapter option:

The VW3A1105 RJ-45 female—female adaptor is used to connect the LCD Graphic keypad and cable. It is not required if using VW3A1112.



ATS480 Remote Mounting Kit