Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the OFS Server V3.63 supported on Windows 11 operating system?
Issue:
OFS Server V3.63 supported on Windows 11 operating system


Product Line:
OFS server


Resolution:
Yes, but you will have to install SP2. Below is the link to download SP2 for the OFS server V3.63.
https://www.se.com/us/en/download/document/OFS_3_63_4904_SP2/

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: