Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If you add the IP55 flange kit NSYPTDS5 to the ATV630 Drive, will it make the drive alone IP55 ratings.

Issue:

If you add the IP55 flange kit NSYPTDS5 kit to the ATV630 drive, will it make the drive IP55 enclosed rated?

Product Line:

ATV630 and ATV930 Drives with the flange kit.

Environment:

Flange kit only

Cause:

Are the Drives IP55 rated with the flange kit?

Resolution:

If the ATV630 or ATV930 Drive is mounted inside an IP55 enclosure along with the optional IP55 flange kit NSYPTDS5 it allows the main enclosure to keep the IP55 rating with the Drive mounted with the flange kit. Note that the ATV630/930 Drive + flange kit does not provide IP55 protection alone the drive has to be mounted inside an IP55 enclosure.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings