Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Ecostruxure Process Expert [2021] : How to rectify the plant SCADA runtime manager services issue
This knowledge base helps the user, when he faces the below issue after launching the plant SCADA runtime manager.

image1

During our investigation, we have noticed the windows user groups for the security roles were not created. As a general practice, we tried reinstallation of plant SCADA and its components which did not help.

Also, we have noticed the security roles weren't created in the plant SCADA configurator.

image

It was found the issue has happened because the plant SCADA was installed on windows system that has Turkish language. There was no notification during the SW installation.

To come out of this issue ,below procedure needs to be followed.
1. Run a command prompt as administrator.
2. Change the current directory to C:\Program Files (x86)\AVEVA Plant SCADA\Security by running the following command:
cd "C:\Program Files (x86)\AVEVA Plant SCADA\Security"
3. Run the following command to initialize the security roles model and add the current user to the roles.
SE.Scada.UACWorks.exe initsecuritymodel "C:\ProgramData\AVEVA Plant SCADA 2020 R2" -adduser
4. Reboot the machine.

The above procedure helps to solve the issue of creating security role model in the configurator and the user will be able to run Plant SCADA runtime without any error.

This issue was seen in plant SCADA 2020R2 version which is a component of EcoStruxure Process Expert 2021.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings