Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Uninstalling Eclipse in Ubuntu
RemoteConnect 3.0.3 works with Eclipse version 2022-06 for the SDK on the Edge platform

If a customer is having issues with Eclipse and needs to repair/reinstall it or if they have an incorrect version installed that needs to be removed.

From a terminal window in Ubuntu (Ctl-Alt-T)

cd ~/
rm -rf ./eclipse
rm -rf ./.eclipse
rm -rf ./oecore-i686/

This will remove all of the components associated with Eclipse. Please refer to the SCADAPack x70 Documentation "Installing Eclipse and SCADAPack 47xi SDK" for reinstalling Eclipse and the SDK.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings