Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to update M580 CPU NTP time via BMENOC0321 module

The CPU time can be synchronized with the NTP time provided by the BMENOC0321 module installed on the same rack. This process is not automatic and requires explicit programming, by following these steps:


1- Enable the "Network Time Service" on the DTM of the BMENOC0321:

BMENOC0321 DTM

2- Open the "Network Time Service " in the service list and put the NTP remote server IP address. You can customise the Polling period, the Time Zone option, etc:


Network Time Service configuration

3- Import the attached program section in your program:

Import section

4- Configure the DFB by putting the module rack position and its IP address:

DFB configuration

5- Use the "Enable" pin to activate the DFB and the Sync_PLC to enable the time synchronization.

6- Enable "Dynamic Arrays" variables in the project settings:

Project settings

The CPU time will be updated after enabling the DFB (via its "Enable" input) AND sending a commande into Sync_PLC input :

Animated DFB

Note: There is no need to enable the CPU’s ‘NTP client’ service.

Best Regards.

Schneider Electric Nigeria

Attachment(s)
NTP_NOC0321.7z [1.82 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: