How can we help you today?

Is It possible to view the free memory space of the BMENOP0300 module ?

It is possible to monitor the free dynamic memory space of the BMENOP0300 module. This feature is available on the module firmware version SV2.6 and higher, with the IEC61850 Configuration Tool V3.3 and higher:

BMENOP0300 firmware history

We can view the free dynamic memory space in the device DDT of the BMENOP0300 module:

BMENOP0300 Device DDT overview

Schneider Electric Nigeria