Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why event ID in TS event buffer could have number 16 ?

1.   Issue :

Why event ID in TS event buffer could have number 16 ?

2.   Product Line :

BMXERT1604T ,BMXCRA31210, BMECRA31210

3.   Environment

All supported Windows OS

4.   Resolution
Event with ID 16 (SOE_UNCERTAIN ) is used to indicate that some events may be lost in the next sequence of events and user needs to check the why the TS buffer of BMXERT1604T (or BMxCRA31210) reaches full state.



Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings