Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is EcoStruxure Control Expert supported on Windows 11 or Windows Server 2022?
Issue:
EcoStruxure Control Expert support on Windows 11 and Windows Server 2022


Product Line:
EcoStruxure Control Expert


Resolution:
EcoStruxure Control Expert V16.0 is now supported on Windows 11 and Windows Server 2022

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: