Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do I need a starting capacitor when using an ATS480 Softstarter?
Issue:
Is there a need for start capacitor on the motor when starting it with ATS480?

Product Line:
ATS480, Altistart 480

Environment:
All

Cause:
NA

Resolution:
A capacitor is not needed when running the motor with an ATS480 Softstarter. The Altistart ATS480 does the soft starting itself.