What lugs can I use with Altivar Process Frame Size 6 drives?
Issue:
Are there lugs available for Altivar 630 and 930 Frame Size 6 drives?
Product Line:
ATV630, ATV930
Environment:
All
Cause:
NA
Resolution:
Please see the ATV930 installation manual and ATV630 Installation manual for lug information on Size 6 drives.
The kit we recommend is "DZ2FH6" and "DZ2FH1" available on SE.com:
Are there lugs available for Altivar 630 and 930 Frame Size 6 drives?
Product Line:
ATV630, ATV930
Environment:
All
Cause:
NA
Resolution:
Please see the ATV930 installation manual and ATV630 Installation manual for lug information on Size 6 drives.
The kit we recommend is "DZ2FH6" and "DZ2FH1" available on SE.com:
Released for: Schneider Electric Nigeria