Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VMware ESXi host reports that the configured guest OS for the PowerChute virtual machine does not match the currently running OS.
Issue:
The VMware ESXi host reports that the configured guest OS for the PowerChute virtual machine does not match the currently running OS.

Wrong-OS-displayed

Product:
PowerChute Network Shutdown versions 4.4.x and 5.x

Environment:
VMware ESXi version 7 and above

Cause:
VMware ESXi host interpretation of the VMs OS.

Solution:
This warning is like an issue reported in VMware knowledge base document 67671. vCenter Server Appliance displays a warning message on ESXi Host Client (67671) (vmware.com ), but it can be ignored as it does not affect the operation of the PowerChute VM.

Note: When the same PowerChute VM is viewed through VMware vCenter Server, the OS is reported as AlmaLinux 64bit Linux.

OS displayed correctly in vCenter Server

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings