Yellow state in the status BAR for all information:
Modification of the memory state (depending on the memory fragmentation state). In BUILT state:
Connected to the Simulator:
In not built state:
UDE APi interface with Read Only mode:
Safety state:
Partial RUN for SAFETY applications (RUN Safe or RUN Proc)
A yellow colored status is meaning something is not correct.
· PROCESS Task RUN (At least one) - SAFE task STOP -> RUN in yellow
· PROCESS Tasks in STOP (All) - SAFE task RUN -> RUN in yellow
Maintenance mode :
No Upload information:
Released for: Schneider Electric Nigeria