Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
DFB's get protected after updating to Control Expert 15.1 or newer
For versions prior to Control Expert 15.1, there could be an inconsistency in the protection of these DFBs, that is, the DFBs in question have a password although there is no protection established for all of them.

Starting with Control Expert 15.1, this consistency was fixed during import (partial and global) in this way:
  • If a DFB has an unprotected password, we force its protection to No Read & No Write.
  • If a DFB has passwordless protection, we set a random password on this DFB and display a prompt in the CE output.
If you need to unlock these DFBs, you can contact Schneider Electric support.