Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I have Vijeo Designer Runtime Windowed?

Issue:
How can I have Vijeo Designer Runtime Windowed?

Product Line:
Vijeo Designer, HMIG5U, HMIG5U2, HMIG5U21, HMIG5U22, Generic Windows PC

Resolution:

In order to view the Vijeo Designer Runtime windowed, please first disable "Windows Key Controls" in the property inspector (Setting will only be visible if the target type is Windows based) and then download to your HMI

Property Inspector

Once the Windows Key Control is disabled, please hit "Control+Shift+V" and it will be windowed instead of full screen:

Windowed RT

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: