Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert - How to run a reconfigure
Issue
Reconfigure lets you rerun the configuration part of the PME install process. Running a reconfigure reverts many of the system settings and components to the install defaults.

Typically, you would use a reconfigure to repair or troubleshoot a damaged system. Consult with Technical Support before running a reconfigure if you are not familiar with the details of this operation.


Product Line
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 9.1
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Power Monitoring Expert

*Warning: Running a reconfigure will revert any Cumulative Updates that were previously installed. The newest cumulative update will need to be run/installed after the reconfigure is completed*

Resolution 1
  1. Open the Control Panel and select Programs and Features.
  2. Select PME within the list of programs.
  3. Click Change in the header area of the list of programs. This opens the installer in maintenance mode.

    reconfigure ui

NOTE: If your system is installed with Windows Integrated Authentication, you can use Reconfigure to change which account is used. To only update the password for the account, run Reset Accounts.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings