The standard delivery is IP40 for K1/K2
Witrh configurator, it is possible to select a gasket (KZ73) in accessories but only for multifixing operating heads with 45X45 front plate (you need to select a label)
For front mounting, the configurator software doesn't propose IP accessories
--> For front plate 45X45, as the reference KZ65 is canceled, I suggest to order it through generic reference GCR_K1S + technical text KZ65
--> For front plate 60X60, the reference KZ66 is still commercialized. It can be ordered separately.
Released for: Schneider Electric Nigeria