Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Upload error "End of Central Directory record could not be found."

Issue

When uploading a history.zip file onPower Advisor (PA),  the upload fails with the error "End of Central Directory record could not be found."

Cause

The cause of the upload failure is due to the absence of source.src in the history.zip file. A typical zip file should contain source.src. Without it, PA cannot determine where to place the uploaded data

Source file

Resolution

  1. Contact the PME application engineer to obtain source.src, which should be automatically generated using the extractor.
  2. Re-upload the zip file with the source.src included.