What is the detail information in BMENOC03x1 Performance diagnostics webpage ?
Issue
What is the detail information in BMENOC03x1 Performance diagnostics webpage ?
Product Line
BMENOC0301 ,BMENOC03011, BMENOC0321
Environment
M580
Resolution
WEB Performance page contains
In the left green block
• Number EIP scanner input Packets per second
• Number EIP scanner output packets per second
• Number Modbus scanner input packets per second
• Number Modbus scanner output packets per second
In the right Client section in blue
• Number Client EIP message activity per second
In the right Client section in red
• Number Client Modbus message activity per second
In the right sever section in blue
• Number Server EIP message activity per second
In the right sever section in red
• Number Server Modbus message activity per second
Released for: Schneider Electric Nigeria