Can a Motor Driven Load be used with an Easy UPS / Back-UPS?
No, an Easy-UPS or Back-UPS use a step-approximated sine waveform on the output of the UPS to the load. The Easy-UPS and Back-UPS models are intened to be used with computers and peripheral devices. These models are not intended to be used with motor driven equipment. If a motor driven load has been attached to the UPS, it may cause premature damage to the UPS.
Please refer to the below extracted from the user manual under troubleshooting section:
Please refer to the below extracted from the user manual under troubleshooting section:
Released for: Schneider Electric Nigeria
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.