Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the terminal block (adaptor) used for LRD4/LR2D4 overload relay to get it mounted on a LC1D115 & LC1D150 contactor?
Issue:
Is LA7D3058 required to mount LRD4 Overload relays on LC1D115 and LC1D150 Contactors?

Product Line:
Contactors and Starters - IEC

Environment:
Tesys D contactors

Resolution:
LRD4*** overload relays don't require any additional terminal blocks to mount directly onto LC1D115 and LC1D150 Contactors. The LRD4*** overload relay is shipped with the adaptor.
LRD4*** Overloads attach beneath the contactor directly.

However, should the adaptor become damaged or lost, the LA7D3058 adaptor is the replacement.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: