Easy-UPS Configuration - Initial Installation
The Easy UPS must be configured with APC by Schneider Electric customer support. This is a one-time process required to be done only during initial installation. The Easy UPS output cannot be turned on without successfully completing the configuration process. After successful completion of the configuration process, the Easy UPS will function normally.
- When the Easy UPS is started up for the first time after installation, the display screen will display 3 numeric digits. “ONLINE”, “ON BATT”, “BYPASS” and “ALARM” symbols on the display get illuminated. All other symbols are not illuminated.
- Contact APC by Schneider Electric Customer Support to obtain the 3-digit Personal Identification Number (PIN).
- Press the ENTER button to enter the 3-digit PIN given by APC by Schneider Electric Customer Support. When the ENTER button is pressed, all the 3 displayed digits change to ‘0’ and the first digit flashes every 1 second. Use the UP-ARROW button to increment the flashing digit or the DOWN-ARROW button to decrement the flashing digit till the first digit of the PIN is displayed. Press the ENTER button to accept the flashing digit and move to enter the second digit of the PIN. Repeat this process till all the 3 digits of the PIN are entered.
- After successful entry of the PIN, a long beep will be heard, and the home screen is displayed on the Easy UPS.
- If the authentication of the PIN fails, then a new 3-digit number is displayed, and steps 2 to 4 have to be repeated.
Released for: Schneider Electric Nigeria
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.