Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the power connection on the M251?
Issue:
Where to connect the power to the M251?

Product Line:
M251

Environment:
All serial numbers

Cause:
Need to remove power for Clone process on M251

Resolution:

The M251 can be powered by using the two methods below:

Power supply
The M251 Logic Controller has a 24 Vdc power supply. It also has a removable screw terminal block with three terminals for connecting the power supply.

USB Mini-B port
The M251 Logic Controller can be powered through the USB Mini-B port to perform limited operations. However, a diode mechanism prevents the logic controller from being powered by both the USB and the normal power supply at the same time.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings