Getting Monitor Circuit error A, B, C or D on a Altivar Process drive
Issue:
Getting a Monitor Circuit error A, B, C or D
Product Line:
ATV930
Environment:
Digital inputs
Cause:
n/a
Resolution:
Suggested to check the digital inputs to see if one of them is assigned to Monitor Circuit A,
B, C or D (Example: if a surge arrestor is assigned to the digital input and is damaged) can cause this.
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
Released for: Schneider Electric Nigeria