How can we help you today?

V321 relay can't export CID file

V321 can't export CID file
Issue
Customer found that Can’t export CID file from V321 relay through Easergy Pro.

_____________________________________________________________
Product Line

VAMP321
_____________________________________________________________

Environment
20.116/20.117
_____________________________________________________________

Root Cause
As the information from R&D team that V321 relay don’t support CID file exporting through Easergy Pro tool in Firmware 20.116 and 20.117, but we will have this function in firmware 20.200, means if we upgrade firmware to 20.200, then we can export CID file from V321 relay through Easergy Pro.
_____________________________________________________________

Solution
When firmware 20.200 is ready, if required, we can upgrade the firmware to 20.200.
_____________________________________________________________

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings