Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to manually delete I/O mapping after deactivating the IEC61850 Server function of a BMENOP0300 ?

If the Server function on the IEC61850 Configurator tool was previously enabled, the related mapped variables are automatically created on EcoStruxure Control Expert Device DDT.

To disable this Server function and delete the related variables on ECE:

  1. Delete first Server variables on the IEC61850 Configurator tool by opening the IEC61850 Configurator tool:

ECE screenshot

2- Click on "I/O Mapping ":

IEDCT tool

3- Select "Server" tab and click on “remove all”, then “yes”:

IO mapping

4- Go back to the «General” tab an disable the Server function:

General tab

5- Close the IEC61850 configurator: It will ask to save > click on 'yes':

close tab

6- Click on “Update application”, then make a "rebuild all" of the program:

Update app

The previous "Server" variable will be automatically deleted on the ECE Device DDT side.