Is there library/function block or template to add ATS480 soft starters to be controlled in Ecostruxure Machine Expert?
Issue:
How to program ATS480 using FB with EcoStruxure Machine Expert?
Product Line:
EcoStruxure Machine Expert
ATS480
Environment:
Ecostruxure Machine Expert
Cause:
There is a DFB and some information for Ecostruxure Control Expert.
Resolution:
There is no specific FB for the ATS480. Also the ATS480 DTM is not integrated yet on Machine Expert.
It is possible to use Generic Modbus TCP Slave for controlling ATS480 (so, no FBs as for ATV).
Released for: Schneider Electric Nigeria