Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot configure the Quantum 140NOC77100 Ethernet IP module.

The Quantum 140NOC77100 Ethernet IP module can be configured in Control Expert or Unity using the attached 'Unity Pro EtherNet/IP Configuration Tool'.

The 'Control Expert' or 'Unity' software must be installed prior to the installation of the 'Unity Pro EtherNet/IP Configuration
Tool'.

'Control Expert' or 'Unity' will need to be started using 'Run as Administrator' in order to open the 'Unity Pro EtherNet/IP Configuration
Tool'.

Schneider Electric Nigeria

Attachment(s)
Ethernet IP Config Soft V1 1.zip [20.68 MB]