Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to solve the EIP device input ddt missing of BMXNOC0401 on Control Expert 16.0 ?

Issue:

How to solve the EIP device input ddt missing of BMXNOC0401 on Control Expert 16.0 ?

Product Line:

M340

Environment:

EcoStruxure Control Expert 16.0

Resolution:

User could install the ControlExpert_V160_HF010 and rebuild the application to solve this issue.
https://www.se.com/id/en/download/document/ControlExpert_V160_HF010/