How can we help you today?

How to View a Geo SCADA DNP3 Device Profile

When Geo SCADA is installed, it creates a folder where it places several DNP3 Device Profile documents.  These DNP3 Device Profile's are documents that describe Geo SCADA's DNP3 capabilities and settings with regards to DNP3 Master and Slave functionality.

The DNP3 Device Profile documents for Geo SCADA are found in the following directory:

C:\Program Files\Schneider Electric\ClearSCADA\InteropDocuments

They consist of the following .xml files:

image1

To view these files, a user must perform the following steps in Microsoft Edge:

1) Open Microsoft Edge, click on the 'Ellipses' button (top right) and select 'Settings'

image2

2) On the next screen, select 'Default browser' (left side of screen)

image3

3) Set 'Allow sites to be reloaded in Internet Explorer mode (IE mode)' to 'Allow'.  Click the 'Restart' button if it appears.

image4

4) Drag the .xml file (I.E. Geo SCADA Expert DNP3 Master Device Profile.xml) onto a new tab in Edge.  The page should appear blank.

image5

5) Again, click on the 'ellipses' button (top right) in Edge.  Select 'Reload in Internet Explorer Mode'.

image6

6) The DNP3 Device Profile should now be displayed properly.

image7

Schneider Electric Nigeria