How can we help you today?

Compatible Solar Panels for APC Portable Power Stations

Issue:
What Solar Panels are compatible with APC Portable Power Stations?

Product Line:

  • Schneider OffGrid Portable Power Station models: PPS330, PPS500, and PPS730

Resolution:

APC Portable Power Stations can be recharged using optional solar panels, which offer a sustainable and portable power solution. Please refer to the following regarding compatibility:

PSP100 100W Schneider OffGrid Portable Solar Panel is compatible with PPS330, PPS500, and PPS730 models.
PSP200 200W Schneider OffGrid Portable Solar Panel is only compatible with PPS500 and PPS730 models.


For any further questions, please contact our Customer Care Center at https://www.apc.com/us/en/support/

Schneider Electric Nigeria