Can I activate the service port mirroring of M580 CPU on the fly ?
Issue:
Can I activate the service port mirroring of M580 CPU on the fly ?
Product Line:
M580
Environment:
M580
Resolution:
User could activate the service port mirroring of M580 CPU in Control Expert ton the fly by following steps :
Online CPU DTM >>Right click CPU DTM >>Click "DTM menu" >>Click "Additional Functions " >>Click "Online action "
Then you could select the source mirroring ports as “YES” and click update to activate the function . After that ,you could select the source port as "NO" and click update to remove the port mirroring .
Released for: Schneider Electric Nigeria