Why the usage of Batch files ofsservice.bat and ofsnoservice.bat is not available anymore in OFS version 3.63 SP3 ?
The usage of batch files ofsservice.bat (resp. ofsnoservice.bat) may be vulnerable and are no more installed.
Solution :
Run instead regofsservice /true (resp. regofsservice /false) in a command line to register (resp. unregister) the server as a service.
Product line :
OFS 3.63 SP3
Environment :
Windows 10 and above
Released for: Schneider Electric Nigeria