Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Configure Control Expert to communicate with the M580 through the BMENUA0100 using HTTPS.

Use the following steps for configuring Control Expert to communicate with the M580 CPU through the BMENUA0100 control port in HTTPS secure  mode.

  • Open the Security Editor.
  • Whitelist the M580 CPU certificate in the Security Editor.
  • Apply the changes.
  • Close the Security Editor.

sdcdsc

  • Open the BMENUA0100 web page.
  • Enable the IP forwarding service.

fgngf

  • Enable the HTTPS service.

eteaht

  • Disable IPSEC if it is not being used.

tgtg

  • Connect to the M580 using the BMENUA0100 control port IP address.

yrhsss

gteag

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings