Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When ION8650 meter is powered up, the display gets stuck on the ION Initialization screen results in loading to the splash screen.

Issue
When ION8650 meter is powered up, the display gets stuck on the ION Initialization screen results in loading to the Splash screen.

Meter is shipped from factory with default Template and when it is powered up, the boot procedure starts with the initialization screen which will lead to default display screen:

Initializing Display

_____________________________________________________________
Product Line
ION8650 series meters
_____________________________________________________________
Cause
1-
For some reason, the meter does not have a Template; for example, during the upgrade, the Template was not uploaded successfully. which can lead to the splash screen being displayed:

Splash Display
When connecting to the meter through ION Setup -> Single ION Device configuration mode, the error message 'No template detected' is displayed.

2- Meter has not been powered up with sufficient recommended voltage as stated in installation guide and meter's Display will be stuck on Initializing screen with series of asterisks that are increasing.

3- Meter is stuck in boot loop and initializing state with asterisks that are not increasing and meter just restarts and repeats the sequence again.
_____________________________________________________________
Solution
1- Load a template onto a meter, this can be done in ION Setup or Power Monitoring Expert.

2- Connect the meter to the recommended Input Voltage range(blade power) or Control Power(auxiliary) to power up and pass the initializing step.

3- Meter needs to be sent to the factory for repair.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: