Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Geo SCADA License Server - Error 1069 - The service did not start due to a logon failure

A ViewX remote client licensed with its own license file needs the “Geo SCADA Expert License Server” service to be running so the license will be recognized and ViewX can connect to the remote Geo SCADA Expert (GSE) server successfully.

It may happen that the “Geo SCADA Expert License Server” service fails to start automatically. A possible cause would be that a corporate group security policy changes some user rights; specifically the "Log on as a service" one.

This can be checked the following way:

In Windows, run the "Local Security Policy" editor and navigate to "Security Settings\Local Policies\User Rights Assignment\Log on as a service". Check that "NT SERVICE\ALL SERVICES" is included. This is required as the license server runs under a Virtual Service Account (VSA).

image1

Log on as Service

The GSE installer ensures that this is configured correctly, but, as mentioned above, something (e.g. a corporate group policy) may change this policy after the installer runs, thus causing this problem.

A trick to repair this issue (tested in Windows 10) is to change the service from log on as "NT SERVICE\LICENCESERVER" to "Local System account" and then back again (leaving the password blank).

NT_SERVICE

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings